查看:
5618
|
回复:
4
|
凌阳凌通电机驱动专用芯片GPM8F3132C上市
|
|||
chen
13
主题
218
回复 |
发表于2018-06-12 15:01:06
|
显示全部楼层
1#
电梯直达
GPM8F3116A购买链接:http://item.szlcsc.com/232704.html GPM8F3132C购买链接:http://item.szlcsc.com/232703.html 资料下载请直接点击GPM8F3116A.pdf (下载次数:0) 资料下载请直接点击GPM8F3132C.pdf (下载次数:0) General DescriptionThe GPM8F3132C family includes two types: GPM8F3132C and GPM8F3132C-QV043. The GPM8F3132C family is a highly integrated microcontroller which integrates a pipelined 1T 8051 CPU, 1K / 8K byte XRAM, 256-byte IDM SRAM and 32K-byte program Flash. It supports up to 35 programmable multi-functional I/Os, Timer0/1/A/B/C, UART0, SPI (master/slaver), I2C (master/slaver), one OP, two comparator, 64MHz PLL, 16-bit X 16-bit multiplier, 32-bit / 16-bit divider, 16-bit adder, 16-bit subtractor, 32-bit shifter and two 8-channel SAR ADCs with 12-bit resolution. It operates over a wide range of working voltage, from 2.4V through 5.5V, in different clock sources. It has one mode in power management unit. Moreover, there is one on-chip debug circuit with two pins to facilitate full speed in-system debug. Features
|
|||
chen
13
主题
218
回复 |
发表于2018-07-03 16:10:05
|
显示全部楼层
2#
自顶一个
|
|||
chen
13
主题
218
回复 |
发表于2020-09-24 12:17:58
|
显示全部楼层
5#
有的,有需要可以联系我,卖你一个,小企鹅3085867220
|
|