查看:
114158
回复: 87 |
DCDC降压芯片, 不需肖特基二极管,电路超简单,2MHZ, 可40V高压输入,几乎是最简...
|
|||
电子工程师
24
主题
331
回复 |
发表于2017-07-25 10:14:02
|
显示全部楼层
1#
电梯直达
DCDC降压转换器, 不需肖特基二极管,电路超简单,2MHZ, 高达40V输入, 几乎是最简单的降压电路。 型号: BL9341 , 是上海贝尔大厂出品的,出货是几万K的,品质相当不错。已经大量在电表,电力,工业,仪表等等领域使用。
2MHZ开关频率,可以使用更小的电感,纹波更小,成本优势明显,节能PCB空间。特别适合模拟信号采样应用要求低纹波的场合。建议配合使用固体铝电解电容或是钽电容,效果更佳! 4.7-40V输入电压,0.6A输出电流,输出电压可调。 DCDC降压转换器, 不需肖特基二极管,电路超简单,我见过最简单的降压电路。 转换效率超高, 带短路、热、欠压、过压等保护。 封装规格:SOT-23-6
DC-DC芯片/ BL9341
采购连接:http://www.szlcsc.com/product/details_94372.html
|
|||
广州电源
11
主题
620
回复 |
发表于2018-01-19 09:45:15
|
显示全部楼层
45#
看到国产芯片,对应到MPS: 12V转5V,用MP1470, 24V转5V,用MP2451或者MP2359 如果更高电压,用MP2494 DCDC芯片是MPS最擅长做的,在设计中要注意详细阅读芯片规格书。 拿MPS的MP1470为例,规格书中明确说了以下四条规则,严格遵循即可: 1) Keep the connection between the input ground and GND pin as short and wide as possible. 2) Keep the connection between the input capacitor and IN pin as short and wide as possible. 3) Use short and direct feedback connections.Place the feedback resistors and compensation components as close to the chip as possible. 4) Route SW away from sensitive analog areas such as FB. 以上芯片,立创商场均有销售,如需技术支持,请直接联系我。 q3397226930
|
|||
广州电源
11
主题
620
回复 |
发表于2018-01-25 15:09:01
|
显示全部楼层
49#
我朋友用贝岭的这颗ic在高温时炸机了,又老老实实地用回MPS了,毕竟一分钱一分货~
q3397226930
|
|||
广州电源
11
主题
620
回复 |
发表于2018-03-22 11:37:23
|
显示全部楼层
56#
推荐搞MP2451
q3397226930
|
|