查看: 16374
回复: 18
推荐通过国家电网认证的RS485芯片-GM3085E,可省2个TVS管

主题

回复
发表于2018-09-05 12:42:23 | 显示全部楼层
1# 电梯直达

GM3085E是杭州捷茂微(http://www.gmmicro.com/ )生产的RS485芯片。

该芯片已经在电表行业大规模使用用超过10年历史,每月出货量超过kkpcs

GM3085E主要特性:

  

   


GM3085E获得了国家电网认证(下面是国家电网认证盖章页):

备注:没有获得国网认证的RS485芯片是不允许在电表上使用。

 



使用普通的RS485芯片,外围电路需要加3TVS管:在AB之间,A和地之间,B和地之间。

   

GM3085E 在芯片内部A和地之间,B和地之间已经加了TVS管。所以使用GM3085E,仅仅需要在AB之间加TVS管。

每个TVS管的价格在0.3-0.6元之间,少加2TVS管可以节省0.61.2.

这么好的芯片,你还等什么,赶快用起来吧。

 

https://item.szlcsc.com/259208.html


主题

回复
发表于2018-09-06 04:23:56   |  显示全部楼层
2#
Do you have a low sleep capable CAN transceiver?

主题

回复
发表于2018-09-06 23:56:55   |  显示全部楼层
4#

>Can interface is on our product roadmap. 

Do you have a target release date? 

We currently use "TJA1042T,118".


主题

回复
发表于2018-09-07 00:01:27   |  显示全部楼层
5#

More Flash MCU.

TI TPS54160 SMPS.

Do you have any SMPS with 60V DC input and low Iq?


主题

回复
发表于2018-09-11 06:42:42   |  显示全部楼层
8#

TI: SN65176BDR,

Intesil: ICL3232IVZ,

CAN Transceiver: NXP; "TJA1042T,118"