查看:
2587
|
回复:
0
|
凌阳凌通电机驱动专用芯片GPM8F3116A上市
|
chen
14
主题
218
回复 |
发表于2018-06-12 14:49:58
|
显示全部楼层
1#
电梯直达
GPM8F3116A购买链接:http://item.szlcsc.com/232704.html GPM8F3132C购买链接:http://item.szlcsc.com/232703.html
General DescriptionThe GPM8F3116A is a highly integrated microcontroller which integrates a pipelined 1T 8051 CPU, 512-byte XRAM, 256-byte IDM SRAM and 16K-byte program Flash. It includes 34 programmable multi-functional I/Os, Timer0/1/2, UART0, SPI (master), Motor control unit with built-in OP and comparators, audio and one up to 8-channel of 12-bit ADC for general-purpose application. It operates over a wide voltage range of 2.4V - 5.5V with different clock sources. It has two modes in power management unit. Moreover, there is one on-chip debug circuit with two pins to facilitate full speed in-system debug. The detail is described in the following sections. Features
|
|