查看:
114
|
回复:
0
|
雷卯推荐多种功率多封装稳压二极管
|
Leiditech
34
主题
0
回复 |
1#
电梯直达
1.稳压二极管工作原理 稳压管,也被称为稳压二极管或Zener二极管,是一种特殊的二极管,其主要作用是提供稳定的电压输出。稳压管的工作原理基于逆向击穿效应。 当稳压管处于正向偏置状态时,其行为与普通二极管相同,几乎不导通电流。但是,当稳压管处于逆向偏置状态时,当电压超过其击穿电压(也称为稳压电压)时,稳压管会发生逆向击穿现象。 逆向击穿后,稳压管的电阻急剧下降,允许大量电流通过。在逆向击穿状态下,稳压管的电压几乎保持恒定,因此可以提供一个稳定的电压输出。这使得稳压管能够在一定范围内抵消输入电压的波动,从而稳定输出电压。 稳压管的稳压电压由其硅材料的掺杂浓度和结构参数决定。通过调整掺杂浓度和结构设计,可以制造出具有不同稳压电压的稳压管。常见的稳压电压包括3.3V、5V、12V等。 需要注意的是,稳压管在工作时会消耗一定的功率,因此需要考虑它的功率承受能力和散热问题,以确保稳压管正常工作并不受损 2.上海雷卯稳压二极管部分产品列表
3. 常见几种稳压电路 1)典型直流稳压电路 稳压二极管主要用来构成直流稳压电路这种直流稳压电路结构简单,稳压性能一般。图所示是稳压二极管构成的典型直流稳压电路。电路中,VD1是稳压二极管,R1是VD1的限流保护电阻。
未经稳压的直流工作电压通过R1加到VD1,由于工作电压大于VZ1稳压值,所以VZ1进入工作状态,输出稳定的直流电压。 2)电子滤波器中的稳压二极管 下图所示是电子滤波器中的稳压二极管应用电路,VD1是稳压二极管,VT1是电子滤波管,C1是VT1基极滤波电容,R1 是VT1偏置电阻。
在稳压二极管导通后,VT1 基极电压被稳定在13V, 其发射极就输出恒定的12V电压了。这个电路在很多场合下都有应用。 3)稳压二极管构成的限幅电路 下图所示是稳压二极管构成的限幅电路。电路中,IC1和IC2是集成电路,VD1和VD2是稳压二极管。
从集成电路IC1的1脚输出信号通过R1加到集成电路IC2的1脚。当集成电路IC1的1脚输出信号幅度没有超过VD1稳压值时,这一信号完整的加到集成电路IC2的1脚上;当集成电路IC1的1 脚输出信号幅度超过VD1稳压值时,幅度超过部分使VD1导通,信号幅度的最大值被限制,达到限幅目的. 部分品牌产品雷卯替代表展示
上海雷卯电子科技有限公司,成立于2011年,品牌Leiditech,是国家高新技术企业。公司研发团队由留美博士和TI原开发经理组建,凭借技术精湛的研发队伍和经验丰富的电磁兼容行业专家,主要提供防静电TVS/ESD以及相关EMC元器件(放电管TSS/GDT、稳压管ZENER、压敏电阻MOV、整流二极管RECTIFIER、自恢复保险丝PPTC、场效应管MOSFET、电感)。 Leiditech围绕EMC电磁兼容服务客户,自建免费实验室为客户测试静电ESD(30KV)、群脉冲EFT(4KV)、浪涌(8/20,10/700 10/1000)、汽车抛负载(7637 5a/5b)和元器件的性能测试等。Leiditech紧跟国内外技术更新脉搏,不断创新EMC保护方案和相关器件,目标方向为小封装,大功率,为国产化替代提供可信赖方案和元器件。 Zener的简介 稳压二极管(又叫齐纳二极管),是一种硅材料制成的面接触型晶体二极管,简称稳压管。此二极管是一种直到临界反向击穿电压前都具有很高电阻的半导体器件。稳压管在反向击穿时,在一定的电流范围内(或者说在一定功率损耗范围内),端电压几乎不变,表现出稳压特性,因而广泛应用于稳压电源与限幅电路之中。稳压二极管是根据击穿电压来分档的,因为这种特性,稳压管主要被作为稳压器或电压基准元件使用。稳压二极管可以串联起来以便在较高的电压上使用,通过串联就可获得更多的稳定电压,称为双向稳压管。 器件功率从0.5W---5W不等。 电压从2.4V ---200V不等。 Information of Zener Zener diode is a surface contact crystal diode made of silicon material. This diode is a semiconductor device with high resistance until the critical reverse breakdown voltage age is reached. In a certain range of current (or in a certain range of power loss), the voltage regulator is almost invariable in a certain range of current (or in a certain range of power loss), which shows a steady voltage characteristic, so it is widely used in the voltage regulator and limiting circuit. The voltage stabilizing diode is divided according to the breakdown voltage. Because of this characteristic, the regulator is mainly used as a voltage regulator or a voltage reference element. A voltage stabilizing diode can be connected in series for higher voltage, and more stable voltage can be obtained by connecting series, which is called a bidirectional voltage regulator. The power of the device vanes from 0.5W-5W. Voltage from 2. 4V to 200. 稳压管Zener的选用技巧 1.Vz稳定电压值需要与应用电路的基准电压值相同 2.Izt稳定电流大于额定稳定电流,稳压效果更好。稳定电流应高于应用电路最大负载电流的50%。 3.Zzt动态电阻:动态电阻越小稳压效果越好 4.IR: 反向漏电流,越小越好。 5.Pd:Zener在工作电路中的Pd不应超过最大耗散功率。 6.根据电路需要选择合适的封装。 1. Vz Zener-voltage value needs to be the same as the reference voltage value of the applied circuit. 2. Izt Zener-current is greater than the rated current for better voltage regulation. The Zener-current should be higher than 50% of the maximum load current of the applied circuit. 3.Zzt : the smaller the dynamic resistance, the better the voltage regulation effect. 4.IR: Reverse leakage current, the smaller the better. 5. Pd: Zener's Pd in the working circuit should not exceed the maximum power dissipation. 6. Selecting the suitable package according to the circuit needs. EMC电磁兼容工程师,就职于上海雷卯电子科技有限公司。
雷卯是专业电磁兼容方案服务和元器件供应商 ,主要提供防静电TVS/ESD以及相关EMC元器件。
|
|